This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910A31A1RSLT changed from 3.6V to 5V input

Other Parts Discussed in Thread: AM3354, TPS65910

When using the AM3354BZCZA80, the matching power supply TPS65910A31A1RSLT was used.
3.6V input to TPS65910A31A1RSLT, I want to switch to 5V input now, but there are concerns:

Although the maximum input on the manual of the TPS65910A31A1RSLT can reach 5.5V, is there any risk in actually inputting 5V? For example, power and heat problems?
Are there other products successfully applied to the 5V input, are there any other suggestions when designing? Can I avoid the risk? If there are other PMIC with 5V input for AM3354, it can also be recommended.
Thank you!