This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM73606-Q1: thermal test results

Part Number: LM73606-Q1


Hello,

Could you help share the thermal test results of LM73606-Q1?

Input: 12V

Output: 5V/6A@500kHz, 5V/6A@2.1MHz, 3.3V/6A@500kHz, 3.3V/6A@2.1MHz

Ambient temp: 25C, 85C. 

Thanks.

Dongbao