Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24090: BQ24090 Charging current is small.

Part Number: BQ24090

hi Engineer:

My circuit diagram is shown in the figure above.

USB plug in to charge the battery.Testing 5V current is only 20mA.The battery is charging at a very slow rate.The current battery voltage is 3.8V.

ISET2 is connected to BATT through 10K resistor. The current is about 20mA.

Is this normal?Or is there any problem with my circuit?

Thanks!!!