This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: LM5176 no load power power consumption

Part Number: LM5176
Other Parts Discussed in Thread: LM5175

Hi Sir,

Our customer used the LM5176, they are think power consumption too high in no load condition.

We are check TI LM5176EVM  If Vout=12V no load condition input have 6V(VIN)*0.125A(Iin)=0.75W(Pin), 24V*0.0634=1.52W, 36V*0.0712A=2.56W.

EN=Low still 24V*0.0059A=0.14W.

How can we improve? Because customer is used battery, They are care this issue.

Does TI have other solution support 9~36V to 12V @ 7~10A?

Why same condition power consumption difference range 0.75W to 2.56W?

Hugo