Part Number: UCC25630-1EVM-291
Hi Ben-san,
My customer want OVP latch and OCP auto restart.
OVP is ok by adding zener Di BLCC to FB. But OCP restart by gradually current decrease is not good.
Please answer to below.
① Output overcurrent protection It seems that it enters the repetition operation (hiccup mode?) Of 1 second pause after operating about 100 ms when entering detection, but is this time ratio fixed?
Also, what is determined by this time?
② If the load is gradually returned to the rated load from the overload protection operation in the previous section ①, what condition change can be captured (what inputs can be monitored) and can be restored?
③ What are the points (caution points) for restoring the output voltage with no problem at rated load from the overload protection operation due to each overload assuming 2 output control (closed loop control output and unregulated output)? Especially in case of large capacity load etc.
④ Overcurrent protection function has OCP 1, 2, 3 and 3 types of operation level, but how do you specifically protect each of them?
A. Since OCP 1 is a peak voltage detection, can it be thought that it can be protected by observation voltage of TP 16 by adjusting the R 13 constant of the evaluation board?
B. Although OCP 2 and OCP 3 are protective detection of average current,
Can this detection value be confirmed from the outside of the IC?
Also, please tell me about the observation method and setting method.
In case
The reason for this question is that static overload and recovery starting point are necessary because confirmation of static operation setting is necessary.