Hi,
I have a 3.3V regulator design with LM25005 straight from Webbench. Power wise it delivers exactly as expected, ripple is low everything works fine. But the other day we did our preliminary EMC-tests and found a lot of emissions that we eventually traced to the LM25005, as everything else on the board is in reset or disconnected. The emissions are quite broad band and get worse the more we load it. In the attached screenshot the load is ca 1A through a 3.3Ohm resistor.
And this is without any load:
This is the schematic:
We have tried several things with various results:
1) Removed C121 made no difference
2) Putting a snubber network across D14 made some difference, but we had to use ca 4Ohms and 10n to get acceptable levels, which is a lot more than the datasheet recommends.
3) Changing the diode D14 also made a difference, but mostly at what frequency the emissions occur.
4) Increasing the inductance from 10uH to ca 100uH made no measurable difference.
Any help is very welcome!
Best regards,
Andreas Wileur