This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25892: 5V "safeout" for CPU VBUS Sense pins

Part Number: BQ25892


Hi,

Via PD (type-c power delivery), we can negotiate lets say 12V VBUS -> the BQ25892

Most CPU's on the market would want 5V for their "vbus sense" pins though. Any tips on ways to solve this, preferably without adding parts...

- a wide-input range LDO could do the job, but then that would have to be muxable so it's isolated in a OTG/host-power scenario

thoughts?