Part Number: UCD9090A
9/15 ICT detectd 2PCS bad boards, the initial analysis was UCD9090A bad, the separate debug digital test item found UCD9090A PIN 9(PMbus) is error, OK board should be low level output, but bad board is high level output, and the same phenomenon occurred in production line on 5/8. At that time, we make A-B-A test and the problem follow material . After sending bad materials to TI factory, the NTF report from the manufacturer.
This time, we use TI tool Fusion Digital 7.1.1 to check UCD9090A and can not detect device ID but ROM mode. There are 2 program Flash checksum(actual& calculated) do not match the OK IC.
How we can take UCD9090A back to detect device ID from ROM mode, then program code again. Thanks!
,