Hi,
Please tell me the recommended eFuse device to meet following requirements.
- 18V input rating
- Up to 3A
- Constant current limit protection
- No reverse current protection
Regarding #4, the customer plan to use eFuse as input current limit for the product with OTG function. So they need to output 5V from OUT to IN of eFuse. I think eFuse without reverse current protection can input 5V to OUT pin and output from IN pin. Is my understanding correct?
Best Regards,
Satoshi