I am looking at the BQ24650 particularly at "converter operation" in the datasheet. I notice that it is mentioned twice in the both "Device Functional Modes," and "Feature Description." These descriptions are on page 13 and page 20 of the datasheet. When describing the converter operation, the description is the exact same for these two sections but in "Feature Description" is mentions an optimal range of 12-17kHz while in "Device Functional Modes" it mentions an optimal range of 17-25kHz. In Feature description, it carries this range forward to give inductor, capacitor and sense resistor recommendations but is this 17-25kHz range something else?
Thanks,
Beau