Other Parts Discussed in Thread: BQ25606
Hi,
There are 2 different input voltage that this device should work that is 12V and 24V.
Now my concern is can I use 24V adaptor directly to charge the 1-cell 3.7V battery, Please suggest?
Is there any thing that need to taken care, because I am using only single cell battery.
Also is there any battery charger IC that will provide regulated power path output, when connected to the external DC input, the IC should have wide input range and should at least support 5V, 3A current to the load.
Please suggest ASAP since I am running out of schedule.
Regards,
Karthik