This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455A: Daisy chain

Part Number: BQ76PL455A
Other Parts Discussed in Thread: BQ76PL455EVM

Hello,dear

I am using the BQ76PL455EVM board, I have a problem to confirm, thank you.

I have completed signle board debugging two days ago .Now,I want to test daisy-chain. But i can‘t connect the second EVM board by  daisy-chain.

I connect the second board in this way : the second board ’s J4 connect to the frist board‘ J5,the WAKE up PIN connect to GND  , the RX and TX PIN connect to VIO .Then ,use BQ76PL455' GUI ,but only can detect one board. How should i do?

regards.

10/5000
Wǒ bùnéng liánjiē qǐ dì èr gè bǎn
I can't connect the second board
  • Hi Sheng Xu,

    1)Please check SW2 setting. For stack EVM, you should set SW2 to diff mode.

    2)You can download sluuba7a_bq76PL455EVM and GUI User Guide, and see section-SW2 for more details.

    3)If it still doesn't work, you can take the second board as base board to check the functionality of the board.

    I think 1)should be the problem.

    Thanks! 

    Andy