This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: TLC5958 sample code

Part Number: TLC5958

Thanks,  

Another, I have a problem need to solve.

Test environment :  Win10  ; CCS 8.1 ; MSP432P401R launchpad

I've had an error while starting program flash or debug. The error message as follows:

CORTEX_M4_0: * WARNING *: The connected device is not MSP432P401R
CORTEX_M4_0: GEL Output: Memory Map Initialization Complete
CORTEX_M4_0: GEL Output: Halting Watchdog Timer
CORTEX_M4_0: Flash Programmer: Reading device TLV failed.
CORTEX_M4_0: Error initializing flash programming: Your XMS432P401R material is no longer supported. We recommend you moving to production-quality MSP432P401R/M silicon by ordering samples at www.ti.com/product/MSP432P401R.
CORTEX_M4_0: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.

How can I fix this problem?  Is this a HW issue or configuration issue?