This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25119: In using LM25119 have some problem consultation.

Part Number: LM25119

Hi,

   
I have several problems in using LM25119 need help.

1.What is the maximum voltage of COMP pin?
2. What is the maximum design power of this IC?
3, how to deal with the actual uneven current of two output when used for interlacing configuration?
4. In the actual debugging, when the output continuously increases the load, the voltage of COMP pin gradually rises, no longer rises after reaching 2V. At this time, the output power is limited.How to continue to increase the output power?
5, CSG and CS pin current detection, only for overcurrent protection function?
6. How do we achieve this IC ramp compensation?
7, could you provide a handbook of common problems for the design of IC power supply for your reference?

Vin:80-130VDC
Constant voltage and constant current output
Vo:62VDC, Io:20A
Efficiency: 96%

many thanks.