If I am powering the UCD9090 with a 3.3V aux supply that is always on, how do I get all the power rails to come back on after the main power has cycled. What I am seeing right now is 12V is the main power used to drive all the power supplies and when that gets shut down all the supplies are turned off, but when 12V turns back on, the supplies don't turn back on.