Hi,
We have designed 24Vdc to 5Vdc supply using LM2576T-ADJ/NOPB IC. Layout and schematic is reviewed by TI.
Problem Observed :
Sometime when we switched ON the unit only LM2576T-ADJ/NOPB part found damage rest components are fine.
Verified by replacing simply LM2576T-ADJ/NOPB with new part and circuit works.
Input parameter :
Output Parameter :
Volateg : 5Vdc connected feedback resistor
Current : 2Amax. but 0.5A current load was connected when problem observed.
For refernce schematic attached.
Concerned area :
1) Inductance 220uH local make
2) Delay circuit connected at Pin 5 and ground because it provides delay at the switing ON the unit.
LM2576T-ADJ/NOPB |