Other Parts Discussed in Thread: TPS7B82-Q1, TPS3851-Q1, TPS3850-Q1
My customer need get Fault signal after stopping feed dog 30ms. I use standard watchdog and setting 30ms window. When getting fault signal, MCU will rest and Must run below 100ms. But customer afraid their MCU couldn't run scussfully and need get the second Fault signal below 100ms. So they have the second time to run again. But our device TPS7B6350 will continue 30ms*8=240ms then give the second fault signal.
customer requirment:
Watch dog period: >=10ms.
Window:35ms.
But need the the second fault signal below 100ms/2=50ms.