Other Parts Discussed in Thread: TPS92515, TPS92518, LM3409
Hello,
We are considering using this part in a camera-based system.
Each camera image requires about 200 to 300 usec for the exposure.
Different images at different times will require slight changes in brightness.
Because of the short capture time for each image, if the PWM cycle lines up such that the LED is OFF for a significant portion of the exposure, there will be a dark strip through the image.
How fast can the PWM cycle be run on these chips?
I already see that there is a maximum 10 bit dimming , so that will help set the minimum ON or OFF Time = (1 / 1024) * (1 / PWM_Freq).
-Michael Hope