This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28610: Thermal shutdown problems- How to reduce the power dissipation in the PWM controller?

Part Number: UCC28610


The problem statement is that our 30W flyback converter has a thermal shutdown in 25°C ambient temperature.

The flyback is located in an enclosure with no air movement.

We are using the UCC28610 to charge batteries at a maximum load of 30 watts from a full-wave rectified 120VAc line voltage.

The flyback transformer has 500uH primary inductance.  At full load, the peak primary current measures, at the peak input haversine voltage (170V), about 1.7Apk, fs=80kHz.

The schematic for the Primary side is virtually the same as shown in Figure 44 found in the UCC28610 Datasheet (revised 9/2015).

We use the same decoupling capacitors, gate drive resistors values, and equivalent diodes.

Vdd is connected to a 15V linear regulator that is powered from the Aux. primary winding.

** What are my options to reduce the power dissipated in the controller to relieve the thermal shutdowns?