This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940: BQ76940

Part Number: BQ76940


Hi again. Regarding your comment: "... Also be cautious of the construction and connection of references to the high current path, "ground" references can move substantially with short circuit..." it is ok to connect the GND to Earth (BAT-) with a net tie right? In the EVM pdf file, the net tie exists (7.2.3 page 44) so I used a net tie as well. In the file attached, the net tie is highlighted with a circle around it within the PDF and JPG files. This can not cause the problem (Microcontroller resets in the event of short circuit) right?

Thanks for your consideration.LFP.rar

  • Hi Arash,
    The net-tie is an excellent way to control the connection, it should work well. The MCU referenced to GND for internal signaling should be good. With low side switching you must have isolation between PACK- and other GND referenced signals. If you have a communication port referenced to PACK- that communication port needs isolation.
    I noticed E1 in the schematic, it is a bad idea in a product since any contamination will bypass the FETs.