Hi,
I am considering creating circuits using the TPS61021A device.
I used WEBENCH to check the operation and select a constant.
However, the result of the phase margin is not output to the WEBENCH of this device.
Is it possible to provide phase margin data to me?
Attach the circuit I am thinking now.
(specification)
VIN: 1.5V to 3.4V
VOUT: 3.0V
IOUT: 700mA
Best regards,