I am using the TPS242X EVM (Evaluation Board) to test some designs using the TPS2421-1 and TPS2421-2, 3-V to 20-V Integrated FET Hot Swap IC's.
I wish to to set the current limit of the circuit to approximately 240mA, and using the given formula in the datasheet Rset = 200kohm/Ifault have calculated that the resistor value I require to set this current limit is 820kohm.
However, using this value of resistor results in an observed current limit of approximately 60mA. I have tried three different devices with the same value of set resistor and get this result with all three. The timing capacitor value used is 1uF to give a 40ms Fault Time, and I am only using a potentiometer as a load at the moment.
Using the given formula above, the Rset should be 3.33Mohm to give a fault current of 60mA.
I have double checked and made measurements on the board to ensure the values selected are what I think they are, and they all look good.
Anyone got any idea why I may be observing this result? Is there some recognised problem with the TPS2421?
Cheers.