This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56628: Delaying Soft Start Time

Part Number: TPS56628


Hi Team,

Customers are requesting to delay the soft start time of this device.
The soft start time of TPS 56628 is fixed, 0.7 ms min., 1.0 m stamp., 1.3 ms max.
Customer is requesting 1.0ms min. ~ 10.0 ms max.
I want to realize accuracy of about 2 ms min. ~ 4 ms max., Considering variations.
Please tell me a good way to realize the delay of the soft start time of this device.

Thank you.

Best Regard,

Toshio Fukumoto