Dear Sirs,
over a long time we design in your LM4040 shunt references.
For one application (ADC reference) we use your LM4040BIM3-2.5. The Load is a ADC refence input. VCC is approx 5,3V. The Rv is 2400 Ohms. parallel to the LM4040 we have a 1 µF capacitor.
In the last time we can observe an output voltage above the nominal tolerance. For the BIM the nominal tolerance is 0,2%. So we can measure by many of our LM4040 output voltage between 2,506 Vto 2,507 V.
This is over the naminal tolerance from 0,2%!
We measure with a calibrated Keithley 2016THD. Room temperature is between 22 - 25 °C.
Various new combination with other RV for Diode operrating current from 100 µA to 15 mA do not change this unaccuracy extremly.
What is the reason for this voltage divergence in the last time?
Thank you and best regards
Martin