Part Number: LM5117
Dear All,
We have designed DC-DC converter using LM5117 IC as per steps given in datasheet. But we are facing some issue while testing it.
Below attached is the schematic.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5117
Dear All,
We have designed DC-DC converter using LM5117 IC as per steps given in datasheet. But we are facing some issue while testing it.
Below attached is the schematic.
Hello,
Thank you for sharing this information and your schematic.
I reviewed the schematic and please see my feedback below. Based on my review, I believe that a potential problem is that the design is unstable. Based on my calculations, I think the Compensation components should be updated and potentially the output capacitors.
1. What are the cpacitance and ESR alues for C1 and C2. I only see 220uF listed. Are both capacitors 220uF? By below recommendations may alter based on this value.
2. RComp (R14) should not be greater than 40kOhm. I recommend using a 4.6kOhm resistor.
3. CCompm (39) should be approximately 10300pF.
3. CHF (C12) should be between 14pF to 145pF with the above two changes.
Attached is the calculator tool with my selections.
Best Regards,
Katelyn Wiggenhorn
Hello Katelyn,
Thank you for your reply.
1) C1 and C2 both are same values capacitors. having ESR 0.20Ohm, with 220uF/50V.
I will update the Rcomp, Ccomp & CHF values as per your recommend, will update you.
Hello,
Thank you for trying this additional test. This is my mistake using the TPS54k calculator, I meant to use the LM5117 calculator. Please see the appropriate recommendations below:
Could you also please share waveforms of SW, VIN, and VOUT of the below two cases: