Other Parts Discussed in Thread: LM27403, LM27402
Hi there,
I want to add a 12V backup power supply for my PC mother board. My target output power is 12V 33A, input from a suitable battery from 10-14.4V.
Because there's no multi-phase buck-boost controller I think, so my proposal is to use cascaded boost and buck controller to derive a 12V output from 10-14.4V input. Do you have better recommendations?
Right now, I am considering LM2642 for the multi-phase buck controller (boost controller is not selected yet), however, space(inductor size and input capacitor size) is not too critical in my application. Do you really recommend multi-phase converter? Or just single phase is OK? My output current is "only" 33A, not crazy values like 56A or so...
Thank you.