Hi TI team,
Now, I am studying to use BQ35100 in ACC mode. I would like to have more explanation about this mode and confirm my understanding of datasheet.
In our application, most of the time our system is in low power and our profile current presents a very quick active current around a few 1-100ms and not exceed 100mA.
Datasheet say: "In this mode, the bq35100 device measures and updates cell voltage, cell temperature, and load current every 1 s and begins accumulating after GAUGE_START is received.[...]"
That why I am seeking that ACC mode could not be able measureour profile current because sampling of this mode is every 1s. Could ACC mode be able to monitor capacity with type of current profile (when current go to high during a few ms)?
Regards,
Alexis.