Hi
The customer intend to use TPS65217 under the following condition.
- Battery is absent
- AC is prioritized over USB
Question
1.
Could AC_EN and USB_EN be turned off automatically if the input absence is detected?
2.
Is it possible that the leak current from USB to AC pin could be flowed when AC_EN and USB_EN are 1? (AC and USB are shorted?)
The reason why they have second question is that they concern possibility of reset
could occur when power input is switched from AC to USB.
3.
Can we switch input from AC to USB without Vsys voltage droped?
BestRegards