Hi Guys , I have use TPS5410-EVM board , and that is good Perfect waveform and good ripple .
But i designe the new circuit for tps5410 which cap and resistor is choice by myself.
then the circuit is like this.
Now i have problem is that if RL is low value which near 0~10 ohm then make high output ripple and two oscillator like picture 
which is almost 1.8MHZ frequency, i don't want this. how can i eliminate this frequency , i only need 500khz freq.
and another question is when i use high ohm which near 330ohm that the osillator is not build.
i use the tps5410evm and i find the high or low res is not effect the output frequency.
so why did the this oscillator build ? please help me thx all guys