Other Parts Discussed in Thread: BQSTUDIO
Hi everyone,
we use the BQ28z610 for a configuration of 2S2P accu cells. But unfortunatly the pack doesn't work like it should.
First of all I updated the ChemID to the correct one (CHEMID 440).
I calibrated the BMS as mentioned in the TR (SLUUA65C) and ran the learning cycle as well.
Both cycle counter increased and update Status has entered "0E" like descriped in "slua777" .
After this the Golden Image was created by loading the customized .gg.csv into the Default.srec and Export it as new golden Image.
I updated a new BMS pcb with this generated Image.
When I started running a test cycle with complete discharge and complete Charge, the BMS did not react on the FC and TC tresholds. Charging was not stopped at reaching the defined voltage of 3600mV. The cell voltages increased until the COV treshold was reached at 3675mV and terminated charging.
Kind regards
René