Other Parts Discussed in Thread: INA240
Hello Team,
I cannot find the FIT number for the DCR010505.
Can you share it and upload in the system for future user?
Thanks,
SunSet
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jimmy,
thanks for the information.
May you also provide the other info that are typically returned on the web?
Such as the one below for the INA240.
Can you make sure that the database is also populated, so for the next time we have the data available online?
|
Part number |
MTBF |
FIT |
Usage temp (°C) |
Conf level (%) |
Activation energy (eV) |
Test temp (°C) |
Test duration (hours) |
Sample size |
Fails |
|
INA240A1MPWTSEP |
1.21x 10 8 |
8.3 |
55 |
60 |
0.7 |
125 |
1000 |
1413 |
0 |
Thanks,
SunSet,
Hi Sunset,
You can contact me at j-hua@ti.com to get more indepth detail and information on this.
From what I've seen the MTBF calculation is derived from a "Device Reliability Prediction" report similar to the one attached. I'd expect the conditions for this value to be based on Case-1 Black Box Estimates (50% Stress, Temp = 55degC, No Device burn-in) but this report does not list the other info you are looking for. 4743.LMZ14201_FIT_MTBF_070518.pdf