This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92640: failing of boot diode

Part Number: TPS92640


Hi,

i have an issue with TPS92640.

The BOOT diode failed and created a shortage. Probably the IC is also damaged.
A replacement of the diode with DFLS1100 got the IC working again.

Specs:
Vin = 48V
Vcc = 10.1V

Over an interface a DMX signal is created to dim the LEDs. Depending on brightness the LED driver are working in

  • Mixed mode at low brightness (PWM Dimming + Analog Dimming [Fix. Value set about 20%]) (600Hz at „PWM_SHUTDOWN_G“) or pure
  • Analog dimming (3kHz at „CURRENT_ADJ_G“)

The output has 5x LEDs CREE XQE-HI, (RED, GREEN, BLUE or WHITE).

I can provide schematics but would like to keep them private.

Do you have an idea about what could cause the problem?

BR,
Stefan