This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Resolution of BQ34Z100-G1

Part Number: BQ34Z100-G1

Hi

This E2E post is related to the past one.

Customer want to use 2mohm sense resistor for Imax=30A/ Sense resolution min=1mA.

Is it possible?

Also, Could you please let me know about your recommendation for deadband setting.

Muk

  • Hi Muk,

    To get the best resolution, they should select the sense resistor to maximize the input range of the ADC (+/-125mV). Using only a portion of the range will reduce the resolution. For this case, I would suggest using 4mohm.

    For deadband setting, it really depends on the application - will it be running at low currents for a large percentage of the time? For a 30A application, I would normally suggest setting the deadband to 10mA, but there are many things to consider. I am attaching a document that discusses the sense resistor and deadband selection process in more detail.

    /cfs-file/__key/communityserver-discussions-components-files/196/Sense-Resistor-Selection-for-Optimum-Battery-Gauge-Performance-_2D00_-3.pdf

    Best regards,

    Matt

  • Hi Matt,
    Thank you for your answer. I appreciate your quickly support!

    Muk
  • Hi Matt,

    Customer have additional question.

    Does 4mohm resistor have really no problem? They have the concern from the description in datasheet as below,

    (Datasheet P29, 7.3.5 Fuel Gauging)

    The bq34z100-G1 measures the cell voltage, temperature, and current to determine the battery SOC based in
    the Impedance Track algorithm (refer to Theory and Implementation of Impedance Track Battery Fuel-Gauging
    Algorithm Application Report [SLUA450] for more information). The bq34z100-G1 monitors charge and discharge
    activity by sensing the voltage across a small-value resistor (5 mΩ to 20 mΩ typ.) between the SRP and SRN
    pins and in-series with the cell. By integrating charge passing through the battery, the cell’s SOC is adjusted
    during battery charge or discharge.

    Thanks

    Muk

  • Hi Muk,

    A 4 mOhm sense resistor is okay. I think this comment in the datasheet is a common point of confusion, so I will look into getting this updated to clarify. For a 30A application, 4 mOhm is a good value.

    Best regards,
    Matt