Part Number: TPS23754
Other Parts Discussed in Thread: TPS2543, TPS23755, TPS23753A, TPS23751
I'm not sure the TPS23754 part is the best choice but I'm looking for something that
- supports Type 1 and Type 2 is a bonus
- support for external input power (from a wall wart) when PoE isn't available
- 5V/2.4A isolated output to feed the TPS2543/7 for fast USB charging
- competes with price and features of the Si3404-A
Any help would be greatly appreciated!
Thanks,
George