Part Number: TPS22916
My customer has doubts of using the TPS22916B or TPS22916C.
1. Is the only difference the rise time? Considering that we are not concerned about the rise but just the discharge time of the load, are both references the same?
2. The TPS22916 would be controling the power to an IC which absolute maximum current wont be more than 250mA and normal use would be around 2mA
3. We need to guarantee that the device is off after 50ms or less
4. The IC has input capacitors of 100pF and 100nF. Do extra capacitors at the output of the load switch?
5. With the mentioned values which input capacitor of the load switch do we need? Thanks..