Part Number: TPS7A49
Hi,
i'm in midst of running some high temp test on TPS7A4901DGN with regulator step down from 12V to 9.3V.
Recently we found thermal issue on this device, my initial suspect that this issue was caused by output current consumption. The measured worst case current consumption was 152mA which exceeded the max current of 150mA. According to datasheet section 8.4 on operating modes, my device should still be functioning since it's still below the Ilim of 220mA since Iout<Ilim condition is still in place. if that's the case what will be the potential risks i may face & any recommended guidelines to follow? Thanks.
Regards,
Leo