Hi,
why Manufacturer Access enter 0010,device can not Enter the shutdown mode? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
why Manufacturer Access enter 0010,device can not Enter the shutdown mode? Thanks!
Hi Batt,
My device diagram is as below, In normal mode,DSG FET and CHG FET already on, voltage at pack pin equals to the BAT, at this time,I enter 0010 in Manufacturer Access,but ( voltage at pack pin< Charger Present threshold) did not meet. Is it the reason why device can not Enter the shutdown mode?tks
1.Is there any other method can turn off CHG FET or DSG FET?can host software(mcu)write 0x46register with sbs cmd? thanks!
2.As I known,device(bq20z75) can enter into shutdown mode when write 0x0010 in Manufacturer Access.
but ,how can host(mcu) control device enter into shutdown mode with command ? we can read FullChargeCapacity(0x10) register with SBS Cmd,but how can access the Shutdown(0x0010)? Ican not find related instructions from TRM