This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq3060 Full Charge Capacity

Other Parts Discussed in Thread: BQ3060

I am a bit confused with the listing for Qmax Cell 0..3 in the bq3060 reference manual. It states that the value of Qmax should be set to be equal or slightly greater tha Full Charge Capacity. I assumed that the Full Charge Capacity, Design Voltage, and Design Capacity were all pack level values. But for the Qmax shouldn't it be at the cell level? So if I had a pack that was 2s2p with 2Ah cell the total capacity would be 4Ah and the Qmax for Cell 0 would be 2Ah.

 

Thanks,

Neel