Other Parts Discussed in Thread: LM358
Hello,
I would like to use the LMZM23601 package to convert from 24V - 12V; However, currently only the "non-adjustable" LMZM23601V3SILR is in stock. I would prefer not to wait until the adjustable version is back in stock so I would like to force the 3.3V version to go to 12V instead. I believe this possible by adding a resistor divider from the output to the FB pin, but I need to know the internal resistance values to account for them in the external resistor divider values.
I couldn't find this information in the datasheet, do you have it available?
Thanks,
Kyle Goodrick