Other Parts Discussed in Thread: LM5175,
Dear Timothy,
May I add a question?
It is Urgent.
I attached about question.
0601.LM5145andLM5175question_181025.pdfCould you check it?
Question
Q1
Is it possible to perform FPWM and frequency SYNC operation with the addition of MOSFET shown below?
Is there no problem?
Q2
Is there a specification of the input capacitance of the SYNC pin when adding a MOSFET?
When 5 kΩ PU, the load of VCC increases by about 1.5 mA, but is there a problem within 20 mA in total with SW operation?
Your answer
"In terms of the LM5145's SYNCOUT signal, the recommendation is to measure the amplitude applied to the LM5175's RT/SYIN pin to verify it does not exceed the specification".
Q3
Is it confirmed by actual measurement?
In case
We are concerned about troubles due to thermal characteristics and product variations.
Q4
Clamping is considered with SBD etc. separately from 3.3 V power supply so that the RT / SYNC pin does not become 3.3 V or higher, but how much is the upper limit of tolerance for 3.3 V?
Q5
Or Csync is set to 1000 pF [From EVM]
How much is the external signal amplitude recommended value?
(To satisfy the RT / SYNC pin voltage upper limit 3.3 V, H threshold 2.1 V min, L threshold 1.2 V max)
Best regard.
Bob Lee.