Other Parts Discussed in Thread: TPS54341
Dear support member,
My customer used TPS54340.
I have a question.
(Question)
Q1
We are considering countermeasures against surge current after TPS54340.
A surge of 30 to 35 A / 800 u to 1 ms occurs as a triangle wave at the rear stage of DCDC.
Is it the output response within range of DCDC?
Does the output voltage drop significantly?
Q2
If the response of Q1 is in time, Does overcurrent protection work?
If there is information such as "There is no problem because overcurrent has ** ms delay"
Could you teach?
Q3
In case Q1 does not make the response over range of DCDC or Q2 takes overcurrent protection,
We believe that there is no other choice but to cope with increasing the capacitor capacity of the DCDC output,
but if you include the tolerance and margin for calculation, it will be required about 4000uF.
Is it OK to increase the DCDC output capacitor so much?
Q4
In case of countermeasures against surge with capacitor capacity increase of DCDC output Since it usually thinks it is about several tens of uF and the start time is about 2 to 5 ms
I think it will take 500 ms to 1 s if 4000 uF.
Does it correct?
Best regard.
Bob Lee.