This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28C42: Adding UV and OV alarms or PGOOD to Flybacks

Part Number: UCC28C42
Other Parts Discussed in Thread: UCC28C45, , LM5036

Hello Sir,

I am designing a Power supply for the following config.

UCC28C45

Vin (Min) (V): 85
Vin (Max) (V): 265
Vout (Nom) (V): 12
Iout (Max) (A): 5
Output Power (W): 60

UCC28C42

Vin (Min) (V): 36
Vin (Max) (V): 75
Vout (Nom) (V): 12
Iout (Max) (A): 5
Output Power (W): 60
Isolated/Non-Isolated: Isolated

I want to raise alarm for under and over voltage in my power supply design. How to do it?

  • Hi Vishal Kakade,
    Under/over-voltage at the input or output?
    Could I ask why you have selected these particular controllers.
    The EVM design for LM5036 looks like a good fit for the spec of your second supply.
    This controller has input under/over-voltage detection built in and will stop operation of the PSU in both cases.
    Thanks
    Joe Leisten
  • Hi Vishal Kakade,
    Since I have no response from you for a few weeks I will mark this thread as resolved. Please feel free to raise another thread if you are still looking for answers.
    Thanks
    Joe Leisten