The TPS40210 data sheet does not show an electrical connection for the thermal pad. In the sample circuit, it is shown grounded. I wonder if requires neither?
Customer would like to run this part without the thermal pad. It won't be for long. He plans to use the HKK version later, but want to work out the bugs first with the cheaper part before placing the high $ on to the board. So - if it's okay, can he run without the thermal pad connected? Thanks.