This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: Will BQ24650 provide power without a battery connected or low battery? I need to be able to use it straight away and dont wait for the battery to get charged. Thanks!

Part Number: BQ24650

Will BQ24650 provide power without a lithium battery connected or low battery? I need to be able to use it straight away and dont wait for the battery to get charged. Thanks!

  • Emilija,

    This device does not have the NVDC architecture . The output of the buck converter is connected to the battery and therefore cannot provide a minimum system voltage that is used to charge the battery. Can you tie your system directly to the panel?