This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24160: BQ24160 EOS Issue

Part Number: BQ24160


Hi sir,        

                 Regarding to the BQ24160, when the DC power input is 5V and BQ24160 are broken by surge/ESD energy,

                 Could you tell us the internal of IC (for example MOS or dc/dc converter) are open or short?

                 It means that IN was opened to the SW or IN was shorted to SW , when the BQ24160 are broken by EOS?

BR,

Jingle 

  • Jingle,

    There are two FETS from IN to SW. Q1a (not shown on block diagram) is the reverse blocking and input current sensing FET. Q1b Is the high side buck FET. Both of those FETs are 20V FETs. The low side buck FET, Q2 is a 12V FET. If the buck converter is running, EOS on IN up to 20V will most likely cause Q2, the low side FET, to short. If EOS is above 20V then Q1a will likely short. I do not have statistical data to support this and so cannot warranty this.