Other Parts Discussed in Thread: UC3825, , UCC28950, UC3842, LM5045
Dear TI,
I have a question about the operation of the UC2825 IC for a Full Bridge Boost converter, with duty cycles above 50% on the alternating PWM outputs OUTA/OUTB. It is listed in the specs that the UC2825 can drive the two outputs up until 80% duty cycle (85% for the UC3825), but I have not found any evidence/applications of this in any of the datasheets/application notes. My application of the full bridge boost converter follows following switch, and component waveforms:
I am questioning whether the duty cycle could be expressed as a function of both of the outputs? Thereby limiting a duty cycle of 85% to be 85/2 for each leg of the H-bridge.
I need overlapping sequences of the complimentary H-bridge MOSFETs due to the Full Bridge Boost topology(see figure above), and it is therefore extremely important that I can have a duty cycle on each output above 50% for correct operation. I am looking for an IC that does this, as well as implements PCMC including slope compensation inputs.
If you can help me figure out if this IC can do this, or alternatively could point me towards any other IC that can do this, I would be most grateful.
Thank you for reading and helping me out!
Best regards,
JC