Part Number: TPS717-Q1
Hi All,
My customer is trying to do sequence control of TPS717-Q1, but there is no MCU to control the EN pin, so they want to use RC delay to control the EN signal.
When checking the datasheet, the EN high level is 1.2V, EN low level is 0.4V, so
- Does EN pin have requirement for the slew rate?
- what's the status of the device when EN signal is between 0.4~1.2V?
- Is it possible to add 10ms time delay by adding RC filter at the EN pin? If yes, Which threshold should customer use to calculate the RC filter parameter
Best Regards
Charles Zhang