This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS549B22: Part with same parameters with <15A required

Part Number: TPS549B22

Hi,

My name is Naveen, we are looking for a Switching DC-DC converter with the following parameters

Vin - >5V
Vout - min 0.7V to Max >=2V
Iout - min >6A to max <15A
PMBus/I2C - Mandatory
Remote Sense - Mandatory

While going through your website, we found that there are many parts available with above requirements but none of them suffice all our requirements. One or the other requirements are not met. If you could suggest us part/s which satisfy our requirements? Closest part is TPS549B22 but the current is 25A.

Naveen