I have a technical question concerning the LMG1210.
In the datasheet is written (section 9.2.2.2 Bootstrap Diode Selection): "For extrem cases, where the low-side FET on time is less than 20ns, TI recommends using small GaN FET as synchronous bootstrap instead of a diode. In this case, TI recommends ... to connect the source of the synchronous bootstrap directly to VDD."
I understand this section so, that I replace the diode with a GaN FET and connect the FET's source to VDD, the drain to the capacitor and the gate to the source. So I just use the FET's (very fast) body diode, right?
But when I do so (using GaN FETs from EPC), the maximum voltage for the high side switch is about 3.3V caused by the reverse drain-source characteristics of the body diode. Or am I understanding something wrong?
Do you maybe have a circuit as an example? Or a GaN FET with which you tested the bootstrap circuit of the LMG1210?
I want to use the LMG1210 with EPC's EPC2111 GaN half bridge.