This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138: which pins can be used as DAC output in UCD3138RJAR?

Part Number: UCD3138

Hi,

customer want to use UCD3138RJAR one pin as a reference output.

in UCD3138 datasheet, there are DACs can be output,

customer want to konw what pins can be used as DAC output in UCD3138RJAR?

thanks.

  • Only the comparators that have a ACOMP_x_OUT_EN bit can be used. So this is D,E,F, and G, but G is not put out on the 40 pin package. So there are 3 :
    pin 2 - AD13 Connected to comparator E
    pin 3 - AD06 Connected to comparator F
    pin 4 - AD04 Connected to comparator D

    Note that the output is primarily intended for test purposes and has a very high output impedance.